Thermal imaging cameras are well-established as valuable inspection tools that help reveal missing insulation, HVAC air flow and equipment issues, radiant heating malfunctions, compromised roofing, and much more. By detecting and locating patterns and sources of heat loss that are invisible to the naked eye, thermal images provide convincing evidence in reports where improvements need to be made and how well they’ve been completed.

Thermal Imaging for Energy Auditing & Building Inspection
Find it with FLIR
Thermal imaging for air tightness and energy efficiency are important quality control measures when building or renovating a home. Heat loss can account for up to 50% of total energy consumption in a building with causes ranging from air leakage through chimneys, attics and wall vents to badly sealed doorways and failing argon gas windows to missing insulation.
Detection and Visualization of Air Infiltration and Exfiltration
Adequate air exchange is important for occupant comfort, health and safety, but most buildings have a far higher rate of air leakage than necessary. The root cause is often poor design and/or construction which allows air to leak in or out. Without thermal imaging, the source of these drafts can be extremely difficult to detect and visualize. But with thermal imager in hand, inspectors and contractors can readily uncover the source of the heat issue, leading to helpful advice on the best improvements and repairs to stop energy loss.
測定の内容をわかりやすい報告書にまとめる
専門的なレポートは、熱検査と発見した問題を顧客が理解するのに大いに役立ちます。FLIR Thermal Studio Proで提供される高度な解析及び意思決定サポートには、豊富な測定ツール、バッチ処理、検査ルートの事前計画機能、カスタマイズされたレポートテンプレートが含まれます。


FLIR ONE Series
The flexibility to inspect the way you want at a price you can afford.