CONTINOUS MONITORING

Thermal Imaging Solutions for Data Centers

Data center maintenance teams have a big share in safeguarding the critical resource that customers and businesses depend upon. Fortunately, they have one secret weapon that enables them to spot issues in an early stage before they turn into big problems: Flir thermal imaging.

The Challenge of Maintaining Uptime

Guaranteeing uptime has become increasingly complex for data centers. With so much mechanical, electrical and electronic infrastructure under one roof, overheating is a major concern, not only because the infrastructure is not using the energy efficiently, but also because overheating can cause a complete shutdown of servers, impacting users around the world, or even data or equipment loss. 

24/7 Monitoring for Critical Systems

Many systems that are critical for the data center’s operation heat up before they fail. Temperature is an important indicator of energy consumption and equipment operation, which is why continuously monitoring electrical and mechanical systems with a thermal camera can be ideal for finding faults that increase power consumption or could lead to failures of electrical systems, cooling equipment, or computing hardware.
80 deg 1.jpg
Fixed-Mount Thermal Camera

FLIR A50/A70 Smart Sensor

HVAC and Cooling Systems

To run smoothly and efficiently, data centers need perfectly air-cooled conditions. Data centers are typically making use of a hot aisle/cold aisle layout principle. Server racks are lined up in aisles with the front sides facing each other. The cold aisles get cold air directly from the Computer Room Air-Conditioning (CRAC) unit from the bottom of the raised floor. The cool air cools down the servers on the racks. Meanwhile, the backs of the servers vent out hot air in the hot aisle, which then returns to the CRAC unit.
data center cooling.png
Thermal Imaging Camera For Continuous Condition and Safety Monitoring

FLIR AX8

Early Fire Detection

Although data center fires are relatively rare, they can have a devastating impact. Data centers may be equipped with fire alarms and firefighting systems, but once a fire starts, asset damage is almost certain. Fixed thermal imaging cameras can identify hot spots before they ignite and provide an early warning response to avoid a full-on destructive fire before assets are harmed or safety is compromised.
Learn more about early fire detection
Fig_03-data center.jpg
Fixed-Mount Thermal Imaging Camera for Condition Monitoring and Early Fire Detection

FLIR A500f/A700f Advanced Smart Sensor

Physical Security

Thermal cameras also help protect data centers' physical perimeter against unwanted intruders or trespassers. These systems offer high contrast, high resolution, and long detection ranges that can see in most adverse weather conditions– such as light rain, fog, smoke, or total darkness. When integrated with video analytics, remote operators can review thermal as well as visible video streams for improved alarm verification and intruder identification.

 

 

Request Info

Optin

By submitting you agree to Teledyne FLIR's privacy policy and cookie policy.