FLIR Launches Addition to High-Performance T-Series Thermal Camera Family

WILSONVILLE, Ore., February 19, 2019 – FLIR Systems, Inc. (NASDAQ: FLIR) launched today a new thermal camera in the high-performance T-Series family, the FLIR T840. The high-resolution T840 thermal camera offers a brighter display and an integrated viewfinder to help electrical utility, plant managers, and other thermography professionals find and diagnose failing components in any lighting conditions, helping avoid costly power outages and plant shutdowns.

Featuring the award-winning design of the FLIR T-series camera platform, the T840 features an ergonomic body, a vibrant LCD touchscreen, and a viewfinder to make it easy to use in any lighting conditions. The 464x348-resolution camera incorporates FLIR advanced Vision Processing, including patented MSX® image enhancement technology, UltraMax®, and proprietary adaptive filtering algorithms to provide customers with enhanced measurement accuracy and image clarity with half the image noise of previous models.

The T840 also offers an optional 6-degree lens that allows accurate temperature measurements on small targets at far distances, such as connectors on overhead distribution lines. Also advanced, on-camera measurement tools unique to newer FLIR T-Series models, such as one-touch Level/Span and precise, laser-assisted autofocus, the FLIR T840 enables users to quickly find problems and make critical decisions easily.

With a 180-degree rotating lens platform, the T840’s ergonomic design helps reduce the strain of full-day inspections and helps users diagnose hard-to-reach components at substations and on distribution lines. The FLIR T840 offers rapid reporting features that help users stay organized in the field. Wi-Fi streaming to the FLIR Tools® app makes it simple to survey issues in real time, while in-camera GPS automatically tags image files with geolocation data to simplify identification and precise documentation.

The FLIR T840 camera is now available for purchase through established FLIR distribution partners. For more information on the FLIR T840, please visit www.flir.com/t840.

                                           -###-

About FLIR Systems, Inc.

Founded in 1978 and headquartered in Wilsonville, Oregon, FLIR Systems is a world-leading maker of sensor systems that enhance perception and heighten awareness, helping to save lives, improve productivity, and protect the environment. Through its nearly 3,700 employees, FLIR's vision is to be "The World's Sixth Sense" by leveraging thermal imaging and adjacent technologies to provide innovative, intelligent solutions for security and surveillance, environmental and condition monitoring, outdoor recreation, machine vision, navigation, and advanced threat detection. For more information, please visit www.flir.com and follow @flir.

Back to top