Keep your high-voltage equipment in peak condition

With high-voltage (HV) electrical equipment, partial discharge (PD) represents an invisible threat that can wreak havoc on critical infrastructure. If left undetected, PD—such as arcing, corona, and surface discharge—can run the risk of causing power interruptions, leading to emergency repairs. These repairs can amount to millions of dollars for remote locations, and are multiple times more costly than planned repairs.

Maintenance workers are now starting to use acoustic imaging to target PD by finding its distinctive sound signature even before equipment fails. The FLIR Si-Series includes a range of acoustic imaging cameras for partial discharge detection in high-voltage systems. These lightweight, one-handed cameras combine advanced signal processing with AI to automatically detect and recognize PDs up to 10 times faster than traditional methods, with minimal training.

 

FLIR Si2-PD and FLIR Si2-Pro

Find partial discharge in high-voltage electrical systems

Efficiently and securely perform non-contact inspections with the FLIR Si2 for PD detection, or the versatile FLIR Si2-Pro, which not only detects PD but also provides acoustic leak detection for indentifying pressurized leaks in compressed air systems, faults in vacuum systems, and CO2 leaks.

See How Acoustic Imaging Works

Why Acoustic Imaging for Partial Discharge Detection

Locate Partial Discharge Quickly

FLIR Si-Series Acoustic Imaging Cameras, offer advanced sound-based solutions for detecting and analyzing industrial issues such as faults, deterioration, and defects, including partial discharge. Remarkably, sound anomalies generated by partial discharge often precede temperature increases that are detectable by thermal imaging cameras. This grants an added layer of early detection for potential future failures.

While it's not uncommon to hear humming or buzzing near power lines, partial discharge is typically beyond the range of human hearing, rendering them exceptionally challenging to pinpoint. This is especially true in noisy work environments with elevated background noise levels. By utilizing a handheld acoustic imaging camera, similar to a thermal imaging camera, users can scan an area and visualize the precise location of ultrasonic sounds generated by partial discharge on a digital image of the inspected components, regardless of whether these sounds are inaudible or concealed by background noise.

Partial Discharge Diagnostics — Essential for Predictive Maintenance

The identification of partial discharge is an indispensable component of an efficient Condition-Based Monitoring (CBM) or Predictive Maintenance (PdM) strategy. Detecting partial discharge at an early stage is critical as it minimizes potential damage to insulators and significantly reduces the risk of equipment failure, consequently, mitigating downtime.

Achieve Quick ROI

The financial rationale for proactively addressing partial discharge is straightforward: it proves to be a far more cost-effective and less disruptive approach to identify and address partial discharge issues, strategically plan scheduled downtime, and undertake necessary repairs and replacements for insulators and electrical components.

 

Request Info

Optin

By submitting you agree to FLIR's privacy policy and cookie policy.

From the Discover Center

Tech Note

Why Microphone Quality Matters More Than Quantity in Acoustic Cameras

Read more
Application Story

Improve Rail Maintenance Shed Efficiency with the FLIR Si2-Pro Acoustic Camera

Read more
Application Story

Detect and Prioritize Railway Brake Air Leaks with the FLIR Si1-LD

Read more
Application Story

Behind the Scenes: How Acoustic Imaging Technology is Helping the Finnish National Opera and Ballet Run Smoothly

Read more
Application Story

Silent Leaks, Resounding Savings: How Acoustic Imaging Is Saving Pennine Healthcare Thousands

Read more
Fundamentals

Detecting Air Leaks and Mechanical Faults in ATEX Zone 22 with the FLIR Si2x Acoustic Imaging Camera

Read more
Whitepaper

Ensuring Optimal Maintenance and Safety in Railroads and Trains with Acoustic Imaging

Read more
Case Study

Leveraging Acoustic Imaging for Proactive Maintenance in Conveyor Systems

Read more