Combat Rising Energy Costs With Thermal Imaging

The global energy crisis is hitting homes and businesses hard across the UK and Europe, with many people feeling their energy costs are spiralling out of control.

According to the Department for Energy, Business and Industrial Strategy, domestic fuel prices in the UK have increased by 60% compared to 2021. And the recent Business Energy Tracker report from Npower Business Solutions shows that 80% of organisations consider energy to be their biggest threat.

So to keep energy costs as low as possible, residents, homeowners and businesses alike need to improve their energy efficiency. But where to start? Many sources of heat and energy leaks are invisible to the naked eye. While you might notice a cold spot, it’s tough to know whether it’s caused by compromised window seals, plumbing leaks, poor insulation, or something else entirely.

That’s why we have developed a wide range of thermal imaging cameras that reveal hidden sources of energy loss. These tools empower you to proactively detect and resolve energy leaks, which can all add up to help you lower bills and increase energy efficiency.

FLIR Missing InsulationMissing-Insulation-thermal.jpg

Gaps in wall insulation  are a common cause of energy loss 

How Thermal Imaging Cameras Help You Find Energy Loss in Your Home

FLIR’s thermal cameras are designed to be affordable and convenient to use. That means you can easily find significant areas of heat loss in your home that you otherwise might never have noticed. 

FLIR ONe

This small thermal camera connects to your smartphone, giving you powerful thermal vision in the palm of your hand. It’s supported by the user-friendly FLIR Home Inspect app, which also offers guidance on what you can do once you’ve identified an issue.

    C5     

category-home electrical-small.JPG

This rugged, pocket-sized thermal imager can help you identify overheating fuses, find air leaks around windows and doors, track plumbing leaks, and more. It connects automatically to the FLIR IgniteTM cloud for handy and secure image storage.

 

FLIR_Line_Ironbow.png

 

For Home inspection professionals

With millions of homeowners and residents struggling with their bills, people are increasingly looking for ways to find and resolve energy loss in their homes. Home inspection professionals can visit a home to diagnose and report problems, allowing you to fix issues and improve energy efficiency. FLIR offers a range of products that combine outstanding functionality with swift reporting software to enable inspectors to reach more customers and deliver real impact. These products allow inspectors to provide the best service, using the best products, to deliver the best results for their customers:

FLIR E8-XT

The perfect tool for diagnosing electrical, mechanical and building problems. It connects to the FLIR Tools app so you can easily share images and findings.

 FLIR E52   

Suitable for professional home inspection, this 240 x 180 pixel thermal detector features streamlined reporting via integration with FLIR routing software, a built-in mic for voice annotation, and is fully compatible with FLIR Thermal Studio reporting software, meaning less time spent crunching images and more time inspecting.

 

FLIR_Line_Ironbow.png

 

Keeping Your Business Running Efficiently

When it comes to business, maximising operational efficiency is vital for controlling energy consumption and avoiding unexpected downtime. FLIR’s condition monitoring tools help businesses of all sizes and sectors to not only identify energy leaks, but even pinpoint invisible performance issues before they become problems, allowing maintenance teams to proactively optimise their business’s energy efficiency:

FLIR Ex-Series  ex-series-grouping.png

Powerful troubleshooting tools for building, electrical, and mechanical applications. With resolution options up to
320 × 240 infrared pixels an 
d the ability to accurately measure temperatures from -20°C to 550°C, the Ex-Series has models to fit your target size, working distance, visual detail needs, and budget.

FLIR Exx-Series 
The FLIR Exx-Series provides exceptional thermal imaging with onboard inspection routing to speed up surveys and simplify reporting.

      flir Si124     

Si124-2X.png

Acoustic imaging that allows accurate identification of pressurised leaks in compressed air systems or partial discharge from high-voltage electrical systems. Specifically designed for industrial use acoustic cameras are heroes in the detection of invisible issues, enabling condition monitoring teams to resolve issues quickly, keep their day-to-day business moving and see off future problems ahead of time.

 

FLIR_Line_Ironbow.png

 

I've found a source of energy loss; what do I do next?

home-inspector-2.png

Energy loss via loft and roof insulation

Detecting heat and energy loss is the first key step in combatting rising energy costs. The next is fixing it to improve your energy efficiency. Therefore, the sooner you identify and resolve your energy loss issues, the more money you’ll save (while reducing your carbon footprint at the same time). Our range of market-leading products allows individuals, inspection professionals and businesses to be confident about where they need to solve energy problems, meaning you can focus your budget in the best way, to bring your energy costs down and increase energy efficiency now and into the future.

Explore our articles to discover practical, budget-friendly ways to insulate your premises, including How to Prepare a Home for Winter and Spot Issues and Tracking Down Hidden Problems During Home Inspections.

Related articles

Fundamentals

Preparing A Home for Winter – Spot Issues with Thermal Imaging to Save on Heating Bills

Read more
Choosing a Camera

Tracking Down Hidden Problems During Home Inspections with Thermal Imaging

Read more
Back to top