Visible vs. Thermal Security Cameras – Which One Do You Need?

Surveillance cameras capture images that help security personnel track intruders as well as verify incidents and classify incidentsGetting effective image quality begins with choosing the right sensor or camera. Two common options are visible and thermal cameras—both are essential for distinct reasons. Here are the key differences and scenarios for using visible and thermal cameras in end-to-end security solutions.  

 

Visible, NIR, and Thermal Sensors 

Conventional surveillance cameras require light to produce images. However, optimal lighting isn’t always available for security applications, especially in outdoor, remote, or rural locationsBy understanding how cameras rely on the various ranges of light within the electromagnetic spectrum, systems integrators can design a video solution that overcomes most image capture challenges.

Electromagnetic Spectrum

The electromagnetic spectrum

Electromagnetic energy has different wavelengths. The human eye can only see visible light on the spectrum, which ranges from 400-750 nanometers in wavelength and appears as different colors.  Traditional security cameras rely on visible light to create detailed color images optimal for target identification, facial recognition, object recognition, and evidentiary-class video for court proceedings. These are the standard for video surveillance and satisfy requirements for most use cases. They are also the most affordable options. 

Meanwhile, near infrared (NIR or just IR for shortenergy is invisible to the naked eyeNIR cameras can see this invisible light, which allows them to deliver bright images in low-light scenarios. These cameras often utilize NIR lasers or LEDs to beam near IR (usually 850-940 nanometers) that the imager can see when it bounces off an object. The primary limitation of NIR cameras is that they still rely on reflected light and generally only produce a black and white image. They tend to have shorter detection ranges and can yield images with poor contrast 

On the other handthermal security cameras detect mid and long wave IR wavelengths that range up to 14 µm and emit heat. Unlike active IR systems, thermal cameras are not dependent on light. They are passive sensors that only detect the heat, or thermal radiation, that is emitted by all objectsCapturing the differences in heat signatures and reflecting these variances in high-contrast images, thermal cameras yield video in total darkness. Conditions that would typically affect visible cameras—poor lighting, shifting light, rain, sun glare, smoke, or reflections—do not affect thermal cameras. For these reasons, thermal cameras are optimal solutions for harsh, rugged environments that require 24/7 monitoring and long-range detection.   

Deciding Factors  

Here are the criteria that systems integrators should evaluate when designing a perimeter security system to determine whether to deploy a visible or thermal camera.  

  • Feature Identification: If the application requires identification of specific features on a target such as clothing color or hair lengthvisible camera is the best option. Outdoor pan-tilt-zoom cameras are often used for this purpose so security operators can follow and identify suspects once a target has been detected  by an analytic camera or radar sensor  
  • Range: If a customer wants to maximize coverage while minimizing the number of cameras installed for cost-savings, camera spacing is criticalThermal cameras become the optimal choice due to their ability to detect objects hundreds of meters away, even in challenging conditions 
  • Environmental Conditions: Sites affected by severe weather that reduces visibility may require a thermal sensor even if the maximum distance to cover is within the range of visible cameras. For example, a visible camera with a 50-meter range may be able to capture images at that distance through light fog, but at night, that same camera would not be able to see at 50 meters. To simplify setup and guarantee visibility, it is better to go with thermal in adverse environmental conditions. 
  • Video Analytics Performance: Ensuring detection while minimizing the number of false alarms is a key pain point in the security industry, especially for applications that are remotely operated by an external security alarm monitoring company. The most demanding scenarios for video analytics will almost always go with thermal. This is because thermal cameras yield high-contrast images—regardless of the lighting or weather condition—that perform better with analytics and lead to more accurate detection. Thermal cameras are also less susceptible to false alarms from sources such as shadows, sun reflections, changing lighting conditions, insects, and swaying foliage.  

 

Key Takeaways 

In summary, visible cameras are the best, cost-effective option to satisfy identification and evidentiary standards for surveillance applications. When specifications require a camera that can’t be compromised by inclement weather, has long detection ranges, and performs well with video analytics at nighta thermal camera is the optimal choice.  

A comprehensive security solution deployed for perimeter surveillance will leverage both thermal and visible cameras. A turnkey system will also employ multi-spectralpan-tilt-zoom cameras with both thermal and visible sensors. These cameras offer valuable color video and in conditions when a visible sensor cannot perform, the thermal sensor provides clear imagesWhen integrated with radar, these cameras slew to the cue of detected target for superior tracking, situational awareness, and threat assessment. All these video operations as well as real-time response protocols can be efficiently managed through a sophisticated video management system or command and control software.   

 

 

Related articles

Choosing a Camera

Bullet vs. PTZ vs. Dome: Which Security Camera Is Right for You?

Read more
Application Story

FLIR Security Solutions Protect Munu, an Endangered South-Western Black Rhino

Read more
Back to top