Register for our Category II Course

October 13-16, 2025 - Auckland (Takapuna Boating Club)

The Level II Infrared Thermography Training Course is designed for the practicing Level I thermographer who is interested in more advanced infrared training. This infrared training course focuses on strengthening and improving thermography skills for condition monitoring and predictive maintenance applications.

Level II Infrared Thermography Training students must have successfully completed a Level I Thermography Training Course and have a minimum of six months field thermography experience. Attendees completing Level II infrared course requirements and a thermography field assignment will receive an ITC Level II Thermography Certification.

 

Course Description

Benefit

  • Reinforce your Level I Infrared Training concepts with refresher material covering the latest infrared camera, technology and thermal imaging application developments.
  • Avoid costly mistakes - ITC experts review and explain the common misconceptions and misapplications of infrared thermography.
  • Expand your thermography knowledge with new, more in-depth concepts in infrared theory, heat transfer and spatial resolution.
  • Learn the basics of predictive maintenance thermography and overall infrared inspection program development. Learn to calculate avoided costs with Excel-based application software (included).
  • Refine your image analysis and interpretation proficiency with in-depth thermal imaging survey and measurement techniques for predictive maintenance applications.
  • Learn to measure emissivity of common materials.
  • See the latest in infrared thermography report generation and IR inspection database and trending software.

 

Recognition

All ITC thermographers are certified against one or more of the following standards:

  • EN473 recommendations for qualification and certification of non-destructive testing (NDT) personnel, as established by the European Federation and accepted by the American Society of Mechanical Engineers (ASME);
  • ISO 9712 specifying proficiency in infrared thermographic testing as related to the qualification and certification of personnel involved in non-destructive testing (NDT), as established by the International Organization of Standardization (ISO) TC 135/SC 7;
  • ISO 18436-8: Requirements for thermography training and certification of thermography personnel in condition monitoring and the diagnostics of machines, as established by the International Organization for Standardization (ISO) TC 108/SC 5.

 

Your Presenter

Dr Ken Jackson has a PhD from the University of New South Wales in Sydney, Australia. His research there included extensive use of Infrared microscopy in the study of catalytic pathways. Dr Jackson has used and trained in Infrared and other analytical techniques for more than 20 years. Dr Jackson is an Certified Level III Thermographer and has been running training courses in Infrared Thermography in New Zealand and Internationally since 1998.

 

For course registration, please contact ken@infraredtraining.co.nz.

 

Don't miss out, register online now!

Back to top