The Latest Technology for Quantifying Gas Leaks

In this recorded webinar, Director of Business Development Craig O’Neill, discussed how the FLIR QL320 is changing the way the oil & gas industry quantifies emissions and how easy it is to use with the family of FLIR OGI cameras. This portable solution is the pioneer in quantifying gas leaks with optical gas imaging, providing results within seconds in the field when tethered or post processed with FLIR Q-Mode when used in hazardous locations. Anyone who uses a FLIR GF620, GFx320, or GF320 can use this tablet to obtain more accurate emissions metrics, inspect difficult to measure components and reduce operational costs.
The QL320 has been tested and can positively measure leaks as low as 100 scc/min for propane and 300 scc/min (11.8 gr/hr, 0.636 SCFH, 228.4 lb/yr) for methane.
A 3rd party campaign conducted by Concawe has determined the accuracy of QOGI to be 30%.
The maximum distance depends on a few factors, such as the lens you are using and the size of the leak. For smaller leaks imaged with the wide angle 23 mm lens, you should generally be somewhere between five and 15 feet (1.5 to 4.6 meters). For larger leaks imaged with the narrow 92 mm lens, the range can be extended out to 210 ft (64 m).
Distance is an important factor in the algorithm to determine Mass or Volumetric readings. It is recommended to be as accurate as possible for these readings. If you are measuring Concentration, distance is not important.
No, because you're telling the tablet or QL mode in the camera what gas you are imaging.
At this time the FLIR QL320 tablet is solely where the software can be installed. It is important to note that this tablet is ATEX rated for Class 1; Div 2 or Zone 2 locations.
Accurate user inputs are critical to producing correct readings. These include polarity, distance, ambient air temperature, gas composition, and wind.
When using the tablet connected or Q-Mode, the camera must run in normal mode.
At this time the software can only be installed on the FLIR QL320 tablet. We will take this request into consideration for the future.
The input User Data temperature is manually entered into the FLIR QL320 or Q-Mode. It can be from the thermo-anemometer (such as the Extech 45158) or another device. It is ideal to get as accurate of a temperature as possible so that the Delta T is captured correctly and the overlay works correctly.
The camera operates by the energy from components in the background and visualizes specific gases with filters that highlight the gas absorption of that specific gas.
There are some regulations that require quantification when using OGI for leak detection and repair. In certain Canadian provinces, for example, the QL320 is approved to meet those regulatory requirements. In the US, there are currently no regulations requiring quantitative OGI but the method is used by some regulatory agencies for inspection and enforcement. Aside from regulatory applications, our customers are using the FLIR QL320 to prioritize leak repairs, determine methane emissions inventory, and determine the dollar value of leak repairs. QL users are also holding manufacturers of products (actuators, hatches, etc.) accountable to stated leak rate ranges.
Use what you think the most prominent compound would be in the gas composition. For example, we use CH4 in many upstream facilities because that's usually the prominent gas, even though it may not be the only compound.
The Q-Mode files are generally 20 seconds in length and comprised of approximately 300 frames (at 15 Hz).
No. The QL320 is designed to work with FLIR GF320, GFx320 and GF620 cameras that are filtered for hydrocarbon gases.
A 3rd party campaign conducted by Concawe concluded that QOGI was approximately 6x more accurate than a TVA.
2° of Delta T is recommended for ideal results.
It is ideal to measure one leak at a time when using the QL320. When a second leak is in the scene of the camera and enters the boundary for measurement, it would not take into consideration the full reading of the leaking component as the origin of the leak (point release) would not be in the center of the screen.
No, the report is in PDF only. The resulting videos are in a non-proprietary AVI file that could be used in a Word document.
Yes, you can change the gas composition chosen in the file and even create a specific composition if desired.
No, neither the FLIR QL320 nor the FLIR camera are Zone 1 certified. You can use the GFx320 with Q-Mode in a Zone 2 area and then perform the measurement in the tablet afterwards.
No, hydrogen cannot be visualized with a GF320 or any infrared camera.
Wind measurement is not critical to be accurate as the FLIR QL320 only has three options: low (under 2 mph/3.2 kph), medium (2-10 mph/3.2-16 kph) and high (above 10 mph/16 kph). You can use an anemometer and put that input into the Q-Mode or tablet.