Reaching new milestones with optical gas imaging

In this recorded webinar, Strategic Business Development Manager Craig O’Neill discusses new OGI technologies from FLIR that will help customers see more gases – at an affordable price!
Webinar highlights include; advances in hydrocarbon emissions imaging; methane mitigation applications within the natural gas supply chain, power generation, renewable natural gas industries, and more.
The QL320 requires an input of the wind conditions. The unit works very will in small windy conditions and this even helps the unit with quantification as it allows movement of the gas. In extremely high wind conditions, the QL320 may have some error in the readings.
FLIR is continually working to address the industry's needs and we will take this into consideration. A large challenge is that the cooled technology cameras have a high cost to manufacture and to keep the quality where the industry expects it makes the product more costly.
Not at this time.
At this time, there is no C1/D2 version of the uncooled OGI portfolio. FLIR will look to address market demands related to the hazardous location classification camera.
The cooled neutrino camera has a low cut off of 3.4 µm which is higher than the normal absorbtion spectra of hydrocarbon gases. For more details on this product, please visit https://www.flir.com/products/neutrino/
The is no defined accuracy for this product but there are many studies done on this product with results related to the products performance. There are multiple factors that can affect the unit's minimum detectable range but we have demonstrated the capability to quantify propane leaks down to 100 scc/min and methane leaks to 300 scc/min. The maximum range is alse dependent on parameters but we have been able to detect methane leaks up to 300 l/min.
Yes, HSM works with any palette.
No. We do not have a unit that can detect H2S.
It is performed in camera on the SD Card with a FLIR Sequence (radiometric) video file.
The lower detection limit is a minimum laboratory leak rate and is the lowest rate that a user can visualize a gas with the unit in a controlled environment.
The camera operates by the energy from components in the background and visualizes specific gases with filters that highlight the gas absorption of that specific gas.
No. The GF77 does not meet US EPA OOOOa requirements. This is something that FLIR will continue to investigate to address the needs of the market.
The GF620 will be offered with 24° FOV and 14.5° FOV lens versions.
Moisture impact is minimal but there is more absorption of H2O in the longwave spectrum (around 7 µm) than in the midwave. This would mean a cooled solution would be better for applications where water may be present.
This is done with a proprietary algorithm from Providence Photonics. The camera itself does not do this and quantification is performed only with the QL320 (in the tablet or post processing wtih Q-Mode).
This is specific to methane.
Yes. We do have a cooled system that is fix-mounted called the FLIR G300a. These cameras have the same detector as the FLIR GF320 but are designed for continuous operation.
No. The GF77 camera will not quantify. That is a feature specific to FLIR's cooled solutions.
The harness is currently available.