Introducing the New GF77 Series

This recorded webinar introduces the new GF77™ Gas Find IR Series. The GF77 uncooled optical gas imaging camera is known for detecting methane. Now with new interchangeable lens options, this camera can detect SF6, ethylene, and ammonia—making it an ideal solution for electric power utilities, food and agriculture, chemical manufacturing facilities, and First Responders. This affordable solution not only locates gas leaks safely, it can also perform accurate thermal inspections.
Anything that involves methane being released into the atmosphere: environmental stewardship, return on investment, safety, etc.
The GF77 is an uncooled camera and requires very little start-up time.
Yes, the same camera body can be used with both lenses.
3-4 hours on one battery charge.
No, this camera is qualitative only, so can't measure the amount of gas being leaked.
The GF77A is currently only available in the 77LR methane version of the camera. It's basically the same camera as the GF77 but with in-field features (battery, touchscreen, etc.) removed and different electronics added.
Both - firefighters may be more interested in the HR version because it can detect amonia leaks, but depending on the situation both lenses can be used by the fire service.
Yes, it can store mpeg videos as well as csq files for later analysis.
The GF77 has the same government classification as the FLIR T-series and Exx-series.
We recommend annual calibration for most users.
No, The LR lens is finetuned to maximize the ability to see methane. It can also see propane but not as well.
Yes. In addition, the Thermal Studio Software suite is included with the camera.
No, the QL320 only works with our cooled hydrocarbon cameras: GFx320, GF620, and GF320.