How to Use a Thermal Camera to Find the Best Basking Lamp Distance & Water Temperature for Red-Eared Sliders And Other Turtles and Terrapins
Ensure your red-eared slider, turtle, or terrapin thrives with perfectly controlled basking and water temperatures. Learn how to use a thermal camera, like the FLIR ONE Edge Pro, to take accurate temperature readings for your reptile’s habitat — no more guesswork!
Let’s be real—if you have a red-eared slider, turtle, tortoise, or any other cold-blooded reptile, you’ve probably stressed about whether their basking area is too hot, too cold, or just plain wrong. I’ve been there. Meet Raphael, my red-eared slider (yes, named after the Ninja Turtle—don’t judge).
Raphael, the red-eared slider ninja turtle.
I wanted to make sure his basking spot was Goldilocks-perfect, not "this is fine" meme-level" of bad.
That’s where the FLIR ONE Edge Pro came in. This thermal imaging camera lets you see actual temperature readings, meaning no more guessing if your turtle’s heat lamp is on point. And since water temperature is just as important as basking heat, I also used it on Raphael’s feeding tank to keep it at the ideal temp.
In this guide, I’ll show you exactly how to use a thermal camera to dial in the best basking lamp distance and water temperature so your turtle is living its best life.
Why Basking and Water Temperatures Matter for Turtles
Most reptiles are ectothermic, meaning they rely on external heat sources to regulate their body temperature. The right basking lamp distance ensures your turtle gets enough warmth without overheating, while maintaining the correct water temperature supports digestion, metabolism, and overall well-being.
If the basking spot is too cold, your reptile may become lethargic and refuse to eat. If it’s too hot, it can cause dehydration and stress. This is why accurately measuring the temperature of the basking area and water is critical.
Ideal Temperature Ranges:
Basking Platform Temperature: 85°F to 95°F (29°C to 35°C)
Water Temperature:
Hatchlings & Juveniles: 78°F to 82°F (25°C to 28°C)
Adults: 75°F to 80°F (24°C to 27°C)
How Far Should a Basking Lamp Be?
Basking Lamp Distance by Bulb Wattage:
75 W bulb: 10 to 12 inches (25 to 30 cm)
100 W bulb: 12 to 14 inches (30 to 36 cm)
150 W bulb: 14 to 18 inches (36 to 46 cm)
To accurately measure both basking and water temperatures here is how to use a FLIR ONE Edge Pro thermal camera for precise heat control.
Equipment You'll Need
Before we get into the setup, here’s the exact equipment I used to ensure Raphael—my red-eared slider—had the perfect basking and water temperatures:
FLIR ONE Edge Pro - A thermal camera that gives accurate temperature readings. (No more guessing!)
100 W Mercury Vapour D3 Basking Lamp with UV-A, UV-V, AND IR - Because heat alone isn't enough-UVB is crucial for calcium absorption and shell health
Adjustable Lamp Fixture - Directs heat efficiently so Raphael gets even warmth
Adjustable Stand for the Basking Lamp – I use an adjustable stand to raise or lower the lamp until the basking spot hits the perfect temperature. It makes fine-tuning the setup so much easier.
for water temperature:
Now, let me explain something about Raphael’s lifestyle—he’s never been a fan of a permanent tank setup. Instead, he lives outside with us and only uses his tank when he needs to feed, wash, or do other turtle business (with me cleaning the tank between each use). He even lets us know when he wants to go in and when he’s ready to come out.
Because of this, I don’t use a water heater—but I still monitor the water temperature to keep it within a safe range of 75°F to 80°F (24°C to 27°C). If the water is too cold, he won’t want to eat, and if it’s too warm, it can cause stress.
FLIR ONE Edge Pro (Again!) – Yes, I also use this to check the water temperature. Just aim it at the water surface or a submerged object (like a rock).
Scratching Post – Turtles shed scutes (the outer layer of their shell), and a scratching post helps him rub off old layers naturally. Plus, it saves my furniture which he was using as his personal scratchers before I got this.
Step-by-Step: Measuring Turtle Basking and Water Temperatures
Step 1: Set Up Your Turtle’s Basking Area
1. Position the basking lamp directly over the platform
2. Use a reptile-specific heat bulb (wattage depends on your setup)
3. Adjust the height so the basking area gets evenly heated
4. Keep the basking platform dry for the most accurate readings
PRO TIP: A UVB bulb is also essential for shell health, so make sure your turtle gets both heat and UVB exposure.
Step 2: Connect & Calibrate the FLIR ONE Edge Pro
1. Turn on the FLIR Edge One and connect it to your smartphone. 2. Allow it to calibrate for precise temperature readings. 3. Set the emissivity to 0.95, which is ideal for organic surfaces like a turtle’s shell or dry basking areas.
Step 3: Measure the Basking Temperature
1. Hold the FLIR Edge One 6-12 inches from the basking platform. 2. Aim it at the spot where your turtle sits. 3. Check the temperature reading:
Too Low (<85°F/29°C)? Lower the light or use a stronger bulb.
Too High (>95°F/35°C)? Raise the lamp or switch to a lower-wattage bulb.
📏 Basking Light Distance Guide:
75W Bulb: ~10 to 12 inches from the platform
100W Bulb: ~12 to 14 inches from the platform
150W Bulb: ~14 to 18 inches from the platform
💡 If your turtle avoids basking, check for cold or hot spots. The FLIR Edge One can show uneven heat distribution, so you can adjust your lamp’s position for better coverage.
Step 4: Check the Water Temperature
Water temperature is just as important as basking temperature. If the water’s too cold, your turtle won’t digest food properly. If it’s too warm, it can cause stress and bacterial overgrowth.
Here’s how to check it with the FLIR Edge One:
1️⃣ Point the thermal camera at the water’s surface. 2️⃣ Check the reading:
Ideal range: 75°F to 80°F (24°C to 27°C)
Too cold (<75°F/24°C)? Use a submersible heater.
Too hot (>80°F/27°C)? Move the tank away from direct sunlight or use a cooling fan.
🐢 For turtles like Raphael: I also check the feeding tank temperature before meals, since turtles digest food best in warm water.
Step 5: Observe Your Turtle & Adjust as Needed
Even with perfect temperature readings, your turtle’s behavior will tell you what’s working:
✅ Signs the setup is correct:
Basking regularly, but not excessively.
Eating normally.
Active and alert.
❌ Signs something is off:
Avoiding the basking spot = too hot.
Always in the water or hiding = too cold.
Open-mouth breathing while basking = overheating.
Adjust your heat sources until your turtle is comfortable.
Can You Use a Thermal Camera for Other Reptiles?
Even though I used this for Raphael, the same technique works for other reptiles like:
🦎 Bearded Dragons & Iguanas – Their basking spots should be around 95°F to 110°F (35°C to 43°C). A thermal camera ensures they aren’t too hot or too cold.
🐍 Snakes – Heat mats can have hot spots. The FLIR Edge One helps check for uneven temperatures inside their enclosure.
🐢 Tortoises – Just like turtles, they need a warm basking area and a cooler retreat zone.
If your pet relies on heat for survival, a thermal camera can help you get it just right.
Final Thoughts: Precision = Happy Turtles
Whether you have a red-eared slider, terrapin, or another turtle, using a thermal camera removes the guesswork from temperature control.
✅ Basking? Scientifically measured. ✅ Water temp? Spot on. ✅ Happy turtle? Absolutely.
If you want to ensure your turtle’s habitat is perfect, a FLIR thermal camera makes it easy and accurate. So go check your setup and give your turtle the best environment possible!